Getting Started

The following steps are required in order to develop your CODESYS project with CODESYS SVN with version control by Apache™ Subver­sion®:

  1. Install the CODESYS SVN package in CODESYS.

  2. Install an SVN server.

  3. Create an SVN repository.

  4. Open your CODESYS project in CODESYS.

  5. Import the CODESYS project into the SVN project archive.

    ⇒ The CODESYS project is saved in the SVN repository.

  6. To edit and further develop the project with SVN version control, the project is edited in CODESYS and then committed to the SVN repository.

A detailed description of these individual steps is located in the following sections.

See also