DTU.GetDateAndTime (FB prefix: gdt)
This function block of the CAA_DTUtil.library reads the realtime clock. It returns the time of the local time zone (i.e. a possible switch to summer/standard time will be regarded)
The current time zone switch can be defined by „DTU.SetTimeZoneInformation“.
If a switch to summer/standard time has become necessary since the last polling of the time, this is done automatically.
At the start of the module the outputs „dtDateAndTime“ and „eTimeZone“ are reset. (DT#1970-01-01-00:00 and RTCLK_UNKNOWN). After successful operation they will contain the current local time.
xExecute |
BOOL |
A rising edge will start the action see: Guidelines for CAA libs |
dtDateAndTime |
DATE_AND_TIME |
Current local time |
eTimeZone |
RTCLK_PERIODE |
Current time zone |
xDone |
BOOL |
Action terminated successfully see: Guidelines for CAA libs |
xBusy |
BOOL |
Module active see: Guidelines for CAA libs |
xError |
BOOL |
Error occurred see: Guidelines for CAA libs |
eError |
WORD |
Error ID for diagnosis (see DTU.ERROR) |