DTU.TODSplit (FB prefix: tods)
The function block of the CAA_DTUtil.library FB provides hour, minute and second from the IEC 6-1131-3 format TIME_OF_DAY.
|
todTime |
TIME_OF_DAY |
Time |
|
uiHour |
UINT |
Hour (0..23) |
|
uiMinute |
UINT |
Minute (0..59) |
|
uiSecond |
UINT |
Second (0..59) |
|
uiMillisecond |
UINT |
Millisecond (0..999) |