This data structure describes errors, which might occur when handling functions of the CAA_File.library. The error range 5100 – 5199 is reserved for the CAA.File.library in the prefix registration for libraries (LibraryRegistry.chm).
|
NO_ERROR |
0 |
No error |
|
FIRST_ERROR |
5100 |
First library-specific error |
|
TIME_OUT |
5101 |
Time limit exceeded |
|
ABORT |
5102 |
Order has been aborted by activating input xAbort |
|
HANDLE_INVALID |
5103 |
Invalid handle |
|
NOT_EXIST |
5104 |
Directory or file does not exist |
|
EXIST |
5105 |
Directory or file already exists |
|
NO_MORE_ENTRIES |
5106 |
No further entries are available |
|
NOT_EMPTY |
5107 |
File or directory is not empty |
|
READ_ONLY_CAA |
5108 |
File or directory is write protected |
|
WRONG_PARAMETER |
5109 |
Wrong parameters |
|
ERROR_UNKNOWN |
5110 |
Unknown error |
|
WRITE_INCOMPLETE |
5111 |
Not all data have been written |
|
NOT_IMPLEMENTED |
5112 |
Not implemented |
|
FIRST_MF |
5150 |
First manufacturer-specific error |
|
LAST_ERROR |
5199 |
Latest library-specifc error |