This function block flushes data from the file system cache to the disk for the file with given file handle hFile. Calling this function block guarantees that data will be stored on the disk.
|
xExecute |
BOOL |
Rising edge: Action start Falling edge: Resets outputs If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError, iError) are present at the outputs for exactly one cycle. |
|
hFile |
CAA.HANDLE |
Handle of the directory or the file |
|
xDone |
BOOL |
Action successfully completed |
|
xBusy |
BOOL |
Function block active |
|
xError |
BOOL |
TRUE: error occurred, function block aborts action FALSE: no error |
|
eError |
FILE.ERROR |
Local library error ID (0: no error; 5101: time out) |