This function of the CAA_Memory.library compares "MemoryBlockA" with "MemoryBlockB". The amount of "uiNumberOfBytes" will be checked.
The function will return 0, if the areas are identical. If not, the position of the first discrepancy occurred will be returned.
|
pMemoryBlockA |
DWORD |
Address of memory area MemoryBlockA |
|
pMemoryBlockB |
DWORD |
Address of memory area MemoryBlockB |
|
uiNumberOfBytes |
UINT |
Number of bytes to be checked |
|
MEM.Compare |
UINT |
Position of first discrepancy, if existent; 0 else. |
Example:
abyMemoryBlockA : ARRAY[0..9] OF BYTE := 0,1,2,3,4,5,6,7,8,9 ;
abyMemoryBlockB : ARRAY[0..9] OF BYTE := 0,1,2,0,4,5,6,7,8,9 ;
->
MEM.Compare(ADR(abyMemoryBlockA),
ADR(abyMemoryBlockB),10) = 4