This data structure describes errors, which might occur during handling functions of CAA_NetBaseServices.library.
NO_ERROR |
0 |
No error |
FIRST_ERROR |
6000 |
First library-specific error |
TIME_OUT |
6001 |
Time limit exceeded |
INVALID_ADDR |
6002 |
Address invalid |
INVALID_HANDLE |
6003 |
Handle invalid |
INVALID_DATAPOINTER |
6004 |
Data pointer invalid |
INVALID_DATASIZE |
6005 |
Data size invalid |
UDP_RECEIVE_ERROR |
6006 |
Error receiving data via UDP |
UDP_SEND_ERROR |
6007 |
Error sending data via UDP |
UDP_SEND_NOT_COMPLETE |
6008 |
Not all bytes could be sent |
UDP_OPEN_ERROR |
6009 |
Could not open udp connection |
UDP_CLOSE_ERROR |
6010 |
Error closing Udp connection |
TCP_SEND_ERROR |
6011 |
Error sending data via TCP |
TCP_RECEIVE_ERROR |
6012 |
Error receiving data via TCP |
TCP_OPEN_ERROR |
6013 |
Could not open tcp server/client |
TCP_CONNECT_ERROR |
6014 |
Could not open tcp connection |
TCP_CLOSE_ERROR |
6015 |
Error closing Tcp connection |
TCP_SERVER_ERROR |
6016 |
Tcp server error |
WRONG_PARAMETER |
6017 |
Wrong parameter |
ERROR_UNKNOWN |
6018 |
Unknown error |
FIRST_MF |
6050 |
First manufacturer-specific error |
LAST_ERROR |
6099 |
Latest library-specific error |