This function block of the CAA_NetBaseServices.library serves to read data from the previously established connection given in hConnection. As long as xEnable is TRUE the handle of the connection is valid. The pointer pData specifies the memory area to write the read data to. szSize defines the max number of bytes to read. When the data was read successfully, xReady is set to TRUE and szCount indicates the actually read number of bytes.
xEnable |
BOOL |
see: CAA Guidelines |
hConnection |
CAA.HANDLE |
Handle of the connection |
szSize |
CAA.SIZE |
Maximum number of bytes to be read; can be retrieved via operator SIZEOF |
pData |
CAA.PVOID |
Target address for the first byte to be read; can be retrieved via operator ADR |
xDone |
BOOL |
see: CAA Guidelines |
xBusy |
BOOL |
see: CAA Guidelines |
xError |
BOOL |
see: CAA Guidelines |
eError |
NBS.ERROR |
Error id |
xReady |
BOOL |
TRUE: Data received FALSE: No data received |
szCount |
CAA.SIZE |
Size of the received data |