NBS.TCP_Write (FB)

 

This function block of the CAA_NetBaseServices.library serves to write data to the previously established connection given in hConnection. The content of the memory area indicated by pointer pData contains the data to be written. szSize defines the number of bytes to be written. When xDone is set to TRUE the data was written successfully.

Input:

xExecute

BOOL

see: CAA Guidelines

hConnection

CAA.HANDLE

Handle of the connection

szSize

CAA.SIZE

Number of bytes to be written; can be retrieved via operator SIZEOF

pData

CAA.PVOID

The address from where the data can be fetched; can be retrieved with the help of operator ADR

Output:

xDone

BOOL

see: CAA Guidelines

xBusy

BOOL

see: CAA Guidelines

xError

BOOL

see: CAA Guidelines

eError

NBS.ERROR

Error id