Like NBS.TCP_Write this function block serves to write data to the previously established connection given in hConnection. Instead of a pointer to the data, this function block expects a handle of the buffer containing the data to be written. The buffer is passed on and not copied like at NBS.TCP_Write.
xExecute |
BOOL |
see: CAA Guidelines |
udiTimeOut |
UDINT |
The time (µs) after which an FB (e.g. requiring an external acknowledgement) aborts operation due to a timeout with error message |
hConnection |
CAA.HANDLE |
Handle of the connection |
hBuffer |
CAA.HANDLE |
Handle of the buffer |
xDone |
BOOL |
see: CAA Guidelines |
xBusy |
BOOL |
see: CAA Guidelines |
xError |
BOOL |
see: CAA Guidelines |
eError |
NBS.ERROR |
Error id |