This function block of the CAA_NetBaseServices.library serves to receive data from the connection given in hPeer. As long as xEnable is TRUE the handle of the peer is valid. The pointer pData specifies the memory area to write the read data to. szSize defines the max number of bytes to read. When data was read successfully, xReady is set to TRUE and szCount indicates the actually read number of bytes. ipFrom and uiPortFrom indicate the IP and port the data was received from.
xEnable |
BOOL |
see: CAA Guidelines |
hPeer |
CAA.HANDLE |
Handle of Peer |
szSize |
CAA.SIZE |
Maximum number of bytes to be read; can be retrieved via operator SIZEOF |
pData |
CAA.PVOID |
Target address for the first byte to be read; can be retrieved via operator ADR |
xDone |
BOOL |
see: CAA Guidelines |
xBusy |
BOOL |
see: CAA Guidelines |
xError |
BOOL |
see: CAA Guidelines |
eError |
NBS.ERROR |
Error id |
xReady |
BOOL |
TRUE: Data received FALSE: No data received |
ipFrom |
NBS.IP_ADDR |
The ip address the data was received from |
uiPortFrom |
UINT |
The port the data was received from |
szCount |
CAA.SIZE |
Size of the received data |