Tab 'CANopen Remote Device - SDOs'
When initializing the CANbus, CODESYS transmits the current configuration settings by using SDOs (Service Data Objects).
In this tab, you configure the necessary SDOs and determine the transmission order of the objects and the actions taken in case of a transmission error.
The object order in this list corresponds to the transmission order of SDOs to the module.
Notice
If the Expert Settings option is not activated for the current device, then only the user-defined SDOs are shown here.
Add SDO |
Opens the Select item from object directory dialog box where all available SDOs are displayed. The chosen object is inserted after the selected object. |
Edit |
Opens the Select item from object directory dialog box and highlights the respective object. You can modify the object parameters or replace the object with another one. |
Delete |
Deletes the selected objects from the list. |
Move up |
Moves the selected object upwards by one entry. |
Move down |
Moves the selected object downwards by one entry. |
Abort if error |
|
Jump to line if error |
|
Next line |
Line number where processing continues if there an error is detected |
SDO Timeout (ms) |
Timeout for the SDO transmission. If the slave does not respond to the SDO request within this time, then the transmission is canceled with a timeout. |
Create all SDOs |
|
Write complete PDO configuration |
|
Dialog box 'Select item from object directory'
This table shows all object directory entries from the device EDS file for each SDO that are writeable and not larger than 4 bytes. Before you add an SDO for selection in the SDO dialog, you can modify its parameters in the fields below the table. In this way, you can also created an SDO that is not writeable in the EDS file by entering a new index/subindex value.
Name |
COB ID of the PDO or the name of the mapped object as it is used in the device description and in the object directory. |
Index |
Index of the object |
Subindex |
Subindex of the object |
Access Type |
|
Data type |
Data type of the object |
Default value |
Default value of the object |
Bit length |
Length of the object |
Value |