CANopen Local Device

 

In CODESYS, a CANopen local device is a slave device that you add directly below a CANbus node in the device tree of a project. Therefore, you can use the CODESYS runtime system as a CANopen slave.

_can_img_device_tree_local_device.png

(1) CANbus node  (2) CANopen local device

See also