Tab 'EtherCAT Slave - Diagnostics History'
This tab reads the diagnostics data (0x10f3 object) of the slave and displays it in a tree structure. In addition, the messages are issued in plain language.
Requirement: The application is in online mode. The attribute DiagHistory in the ESI file is set.
|
Update history |
The data is read again and the view is refreshed. New messages are displayed in the Flags column with N (New). Acknowledged messages with Q. |
|
Automatic update |
The data is updated automatically. |
|
New messages only |
Acknowledged messages are not displayed. |
|
Acknowledge messages |
All messages with the N flag are acknowledged. In the process, the flag changes to Q. |
See also