Generic connection (free configurable)
The dialog contains the parameters for the new connection.
Automatically generated path |
The Connection path is generated automatically from the values for Configuration assembly, Consuming assembly, and Producing assembly. |
User-defined path |
The Connection path is entered manually in the corresponding input field. |
Path defined by symbolic name |
The path is specified by a symbolic name. Requirement: The device must support connection tags. |
Connection path |
The connection path is used for addressing one or more objects in the adapter that keep the input data ready and receive the output and configuration data. Requirement: The connection path is set to User-defined path. |
Symbolic name |
An ANSI string is used instead of the normal connection path. Refer to the manual of the respective EtherNet/IP adapter for permitted ANSI strings. Requirement: The connection path is set to Path defined by symbolic name. |
Trigger type |
|
Transport type: |
Details for this can be taken from the specifications CIP Volume 1 and Volume 2. |
RPI (ms) |
(Requested Packet Interval) Length of the time interval (in milliseconds) in which the transmitting application requests the transmission of data to the target application. This value must be a multiple of the bus cycle task. |
Timeout multiplier |
In case of device failure, there is a time delay (RPI * Timeout multiplier) before the device state switches to "Error". |
Predefined connection (EDS-File)
Use this option to employ existing connections from an EDS file. The data that can be changed are defined in the EDS file.
O--> T size (bytes) |
Amount of data from the scanner to the adapter |
Proxy config size (bytes) |
Size of the proxy configuration data |
Target config size (bytes) |
Size of the target configuration data |
Connection type |
Refer to the specifications CIP Volume 1 and Volume 2 for details of the parameters. |
Fixed/Variable |
|
Transfer format |
|
Inhibit time |
T--> O size (bytes) |
Number of data from the adapter to the scanner |
Connection type |
Refer to the specifications CIP Volume 1 and Volume 2 for details of the parameters. |
Fixed/Variable |
|
Transfer format |
|
Inhibit time |
See also