CODESYS runtime system as EtherNet/IP scanner
CODESYS provides two different EtherNet/IP scanners:
(1): a device that you insert directly below each network adapter. A CODESYS Ethernet/IP scanner (IEC) can be an adapter at the same time. Functionally this is an originator and a target in one device.
(2): a device that needs a special cifX card.
You insert one or more EtherNet/IP targets below a scanner.
See also