Tab 'ModbusTCP Slave - General'
This tab includes the basic settings for network communication.
Slave IP address |
|
Response timeout |
Time interval for the master to wait for the response from the slave. This is especially configured for this slave node and overwrites the general response timeout setting of the respective master. |
Port |
Port number (TCP/IP) of the slave 502 is default for Modbus |
Note
The communication settings can be changed at runtime using the method UpdateCommunicationSettings. This method is available for the implicitly generated function block of this Modbus slave.
See also