PROFIBUS DP Master - 'General'
This tab defines the network interfaces of the PROFIBUS DP master. The parameters are defined in the device description file, but they can be edited in this dialog.
Station Address |
Permitted range from 0 to 126. Every new device inserted into the bus is assigned an incremented address automatically. Note: Address 126 is the default DP slave address. Addresses are checked for duplicates. |
Highest Station Address |
The highest station address (HSA) on the bus. To attain a stricter GAP range, you can indicate a lower address here. GAP range: Address range that is scanned for new active devices. |
Auto Clear Mode |
|
Automatic startup |
Caution: Whether or not the setting is evaluated depends on the driver. |
Groups |
Opens the Groups dialog. Refer to the description for the Groups dialog. |
These parameters define the time response of communication on the PROFIBUS. |
|
Baud Rate [kBits/s] |
The baud rates defined in the device description file (GSD file). However, you can set only the baud rate that is supported by all slaves. |
Use Defaults |
|
T_SL |
"Slot time" [tBit]: Maximum time interval that the master waits for the first signs of a response from the slave after transmitting a request. |
min. T_SDR |
Minimum "station delay responder time" [tBit]: Minimum response time that a device can respond on the bus (min. 11 Tbit) |
max. T_SDR |
Maximum "station delay responder time" [tBit]: Maximum time interval that a slave has to respond. |
T_QUI |
Idle period which must be taken into account during conversion of NRZ (Non Return to Zero) signals to other codings (switchover time for repeater) |
T_SET |
"Setup time" [tBit]: Time for setup |
T_TR |
"Target Time for Rotation" [Tbit]; projected time interval when a master should receive the token. Result of the sum of the token stop times of all masters on the bus. |
Gap |
GAP update factor G: Number of bus cycles after which the masters GAP (address range from its own bus address to the address of the next active station) is searched for an additional, recently inserted active station. |
Retry limit |
Maximum number of repeated request attempts by the master when it has not received a valid response from the slave |
Slave Interval |
Time between two bus cycles when a slave can process a request from the master (time base: 100µs). The value here must agree with the specifications in the GSD files of the slave. |
Poll timeout |
Maximum time when the response from the master must be received by the requester in a master-master communication (DP_Master class 2) (time base: 1ms). |
Data control time |
Time [ms] when the master communicates its operating status with the assigned slaves. At the same time, the master monitors whether at least one data exchange each has taken place with the slaves within this period, and updates the Data_Transfer_List. |
tBit: Time unit for transmitting a bit on the PROFIBUS; inverse value of the transmission rate (for example, 1 Tbit at 12 Mbaud = 1/12,000,000 bps = 83 ns).
See also
In this dialog, you can assign the slave to one or more of eight possible groups. The groups are used for synchronizing the data exchange between the master and slaves. You can double-click the group names for editing.
Sync |
|
Freeze |
|