This tab shows the diagnostics data and the alarms of the module.
Diagnostics data |
The diagnostics currently located in the device. The current diagnostics data is reloaded from the status display as long as a link can be established to the device. |
Alarms |
All alarms of this module that have been reported by this device since the start of the application. The alarms are stored in a ring buffer on the controller. |
Confirm |
Deletes the alarms from the ring buffer. |
See also