Command 'Multiply visualization element'
Function: This command opens the dialog box Multiply visu element to configure the multiplication of a template element.
Call: Menu bar: Visualization ; context menu
Requirement: The visualization is active and a configured template element is selected.
Dialog box 'Multiply visualization element'
When multiplying, CODESYS inserts additional elements that originate from the template element. CODESYS inserts the new elements as a table, column, or row.
In this dialog box, you configure the multiplication of elements and the arrangement of multiplied elements.
CODESYS inserts the multiplied elements as a table. . |
|
Horizontal |
Number of elements per row Corresponds to the amount of array components in $FIRSTDIM$ |
Vertical |
Number of elements per column For two-dimensional arrays, this information corresponds to the value in $SECONDDIM$. |
|
|
Horizontal |
Row distance between elements (in pixels) |
Vertical |
Column distance between elements (in pixels) |
From top left |
Origin for the arrangement of elements. The configured Arrangement of elements and the configured Orientation are displayed in the Preview window. |
From top right |
|
From bottom left |
|
From bottom right |
Line by line |
Table padding by row or column. The configured Arrangement of elements and the configured Orientation are displayed in the Preview window. |
Column by column |
Start index |
|
Increment |
Interval to increment the respective index Preset: 1 |
See also