Dialog 'Options' - 'Visualization'
Function: The dialog is used for configuring the visualization editor and at runtime of the configuration of the integrated visualization.
Call: Menu bar: Tools ‣ Options (Visualization category)
See also
Note
These settings are not used for the following display variants: CODESYS TargetVisu, CODESYS WebVisu, and CODESYS HMI.
Presentation Options (Visualization editor in the programming system)
|
Fixed |
The visualization retains its original size. |
|
Isotropic |
The visualization retains its proportions. |
|
Anisotropic |
The visualization resizes to the window in the development system. |
|
Use scaling options for dialogs |
|
|
Antialiased Drawing |
Hint: If a horizontal or vertical line is drawn blurry on a specific visualization platform, then this can be corrected by an offset of 0.5px in the direction of the line thickness (see element property Absolute movement, option Use REAL values). Requirement: The platform in use supports using REAL coordinates. |
|
Device image |
If the device image (DeviceImage) is defined in the device description of the controller, then it can be displayed in the visualization editor. |
|
Show offline |
|
|
Show in visualizations with parameter interface |
For visualizations with a parameter interface, they are used often only as a partial image. It does not make any sense to display the device image there. |
|
Show online |
|
|
Link to toggle/tap variable where appropriate |
If you drag an element into the visualization editor that has the properties Color variables and Toggle color, then this property is property is configured with the placeholder <toggle/tap variable>. The following elements are affected: Button, Frame, Image, Line, Pie, Polygon, Rectangle, Text field, Scrollbar. |
See also
|
Visible |
|
|
Active |
The grid lines can be active and also hidden. |
|
Size |
Distance between grid lines (in pixels) |
|
Text list files for textual "List components" |
File name and location of a file of type .csv. It contains a table with texts in a text list format. The file entries are provided when the "List components" feature is used as input assistance. Note: You create this file as an export file of the global text list with the command Import/Export Text Lists. |
|
Visualization Directories |
|
|
Text list files |
Locations for text lists. Note: This setting is valid in the project as long as no other location is configured in the Project Settings (category Visualization, Text list files). Note: The storage location can also be defined by an environment variable. |
|
Image files |
Directory with image files that are available in the project. Multiple directories are separated by a semicolon. CODESYS uses the directory for image pools with image files that are not integrated in the project, but rather referenced by a link. Absolute paths are used for cross-project global images. Relative paths (example: .\\images) are used for project-specific images. This option allows for image pools to be opened successfully if the project and the respective image directory are moved to another directory on the computer. Note: This setting is valid in the project as long as no other location is configured in the Project Settings (Visualization category, Image files). Note: The storage location can also be defined by an environment variable. |
See also
Device setting for libraries and global visualizations
|
The following settings are used when the visualization is in the POUs view or when you are developing a library in a currently open library project. |
|
|
No limitation by device settings |
|
|
Use settings of the following device |
|
|
Currently selected device |
Device whose device settings are used. |
|
Name |
Example: CODESYS Control Win V3 |
|
Version |
Example: 3.5.11.0 |
|
Select device |
Opens the Select device dialog. All installed devices are listed there. You can filter by device or manufacturer. Select a device and click OK to close the dialog. |
|
Derive device automatically |
"Try visualizations; derive the device from current project".
|