Visualization Element 'Combo box array'
Tag: Common controls
The element shows values of an array as a drop-down list. When the visualization user clicks an entry, the array index of the entry is written to an integer variable.
Element name |
Optional Hint: Assign individual names for elements so that they are found faster in the element list. Example: List_Product_Number |
Type of element |
Combo box array |
The position defines the location and size of the element in the visualization window. These are based on the Cartesian coordinate system. The origin is located at the upper left corner of the window. The positive horizontal x-axis runs to the right. The positive vertical y-axis runs downwards.
X |
X coordinate of the upper left corner of the element Specified in pixels. Example: 10. |
Y |
Y coordinate of the upper left corner of the element Specified in pixels. Example: 10. |
Width |
Specified in pixels. Example: 150 |
Height |
Specified in pixels. Example: 30 |
Note
You can also change the values by dragging the box symbols () to other positions in the editor.
See also
The properties contain fixed values for the coordinates of the point of rotation. This point of rotation is shown as the symbol. The point is used as the center for rotating and scaling.
X |
X-coordinate of the point of rotation |
Y |
Y-coordinate of the point of rotation |
Note
You can also change the values by dragging the symbols () to other positions in the editor.
Variable |
At runtime, saves the array index of the list entry that the user clicks
|
Data array |
Displayed as combo box. Every array component becomes a combo box entry.
|
See also
The "Combo box – Array" element visualizes an array variable or structure variable in a tabular view. The index of array elements or structure members is shown in a column or row. Two-dimensional arrays or structure arrays are shown in several columns. You specify the visualized variable in the Data array property. If a variable is assigned there, then you can specify the display of the table columns where the array elements are shown. You can customize each column that is assigned to an index [<n>].
Columns
|
Due to the structure of the variable that is defined in Data array, CODESYS determines the number of columns and defines them with the index <n>. Example: StringTable : ARRAY [0..2, 0..4] OF STRING := ['BMW','Audi','Mercedes','VW','Fiat', '150','150','150','150','100','blue','gray','silver','blue','red'];: three columns are formed [0], [1] and [2]. |
Max. array index |
Optional. Variable (integer data type) or value. Defines up to which array index the data is displayed. |
Row height |
Height of the rows (in pixels). |
Number visible rows |
Optional. If the array is larger than the number of visible rows, then a scrollbar is included. |
Scrollbar size |
Width of the vertical scrollbar (in pixels). |
Element property 'Columns: Column [<n>]'
Width |
Column width (in pixels). |
Image column |
|
Image configuration |
|
Fill mode |
|
Transparency |
|
Transparent color |
When the Transparent property is enabled, the color specified here is not displayed. Pixels with this color are transparent. |
Text alignment in column |
|
Tooltip |
Character string (without single straight quotation marks) that is displayed as the tooltip of an element in runtime mode Example: Products of customer A Hint: The text is accepted automatically into the GlobalTextList text list and can be localized there. |
See also
Element property 'Text properties'
The properties contain fixed values for the text properties.
Usage of |
|
Individual text properties Requirement: The Individual settings text property is defined. |
|
Font |
Example: Default
|
Font color |
Example: Black
|
Transparency |
Whole number (value range from 0 to 255). This determines the transparency of the respective color. Example: 255: The color is opaque. 0: The color is completely transparent. Please note: If the color is a style color and already has a transparency value, then this property is write-protected. |
Element property 'Absolute movement'
The properties contain IEC variables for controlling the position of the element dynamically. The reference point is the upper left corner of the element. In runtime mode, the entire element is moved.
Movement |
||
X |
Variable (numeric data type). Defines the X position (in pixels). Example: PLC_PRG.iPos_X. Increasing this value in runtime mode moves the element to the right. |
|
Y |
Variable (numeric data type). Defines the Y position (in pixels). Example: PLC_PRG.iPos_Y. Increasing this value in runtime mode moves the element downwards. |
|
Rotation |
Variable (numeric data type). Defines the angle of rotation (in degrees). Example: PLC_PRG.iAngle1.
The midpoint of the element rotates at the Center point. This rotation point is shown as the In runtime mode, the alignment of the element remains the same with respect to the coordinate system of the visualization. Increasing the value rotates the element to the right. |
|
Interior rotation |
Variable (numeric data type). Defines the angle of rotation (in degrees). Example: PLC_PRG.iAngle2. In runtime mode, the element rotates about the point of rotation specified in Center according to the value of the variable. In addition, the alignment of the element rotates according to the coordinate system of the visualization. Increasing the value in the code rotates clockwise.
The rotation point is shown as the Note: If a static angle of rotation is specified in the Position ‣ Angle property, then the static angle of rotation is added to the variable angle of rotation (offset) when the visualization is executed. |
|
Note
You can link the variables to a unit conversion.
Note
The X, Y, Rotation, and Interior rotation properties are supported by the "Client Animation" functionality.
See also
Element property 'State variables'
The variables control the element behavior dynamically.
Invisible |
Variable (BOOL). Toggles the visibility of the element. TRUE: The element is not visible at runtime. |
Deactivate inputs |
Variable (BOOL). Toggles the operability of the element. TRUE: User inputs do not have any effect in runtime more. The element is shown as deactivated. |
Note
The Invisible property is supported by the "Client Animation" functionality.
See also
These properties are available only when you select the Preview: Support client animations and overlay of native elements option in the Visualization Manager.
You can animate a movement, a rotation, and the visibility of a visualization element.
Animation time |
Time that the element executes an animation (in milliseconds) Example: 500 |
Move to the foreground |
Property value (BOOL) TRUE: At runtime, the element is displayed in the foreground. FALSE: At runtime, the element is displayed in the layer where it was inserted in the visualization editor. |
See also