Visualization Element 'Potentiometer'

 

Symbol:

_visu_img_potentiomenter.png

Tag: Measurement controls

The element displays the value of a variable as a setting on the potenti­ometer. A visualization user can modify the value by dragging the pointer to another position.

See also

Element properties

Element name

Example: GenElemInst_1

Type of element

Potentiometer

Variable

Variable (numeric data type). Contains the position of the pointer for the potentiometer.

A visualization user can modify the value by dragging the pointer to another position.

Element property 'Center'

The properties contain fixed values for the coordinates of the point of rotation. This point of rotation is shown as the _visu_icon_center_point.png symbol. The point is used as the center for rotating and scaling.

X

X-coordinate of the point of rotation

Y

Y-coordinate of the point of rotation

Note

You can also change the values by dragging the symbols (_visu_icon_center_point.png) to other positions in the editor.

These properties are available only when you select the Preview: Support client animations and overlay of native elements option in the Visualization Manager.

You can animate a movement, a rotation, and the visibility of a visualiza­tion element.

Animation time

Time that the element executes an animation (in milliseconds)

Example: 500

Move to the foreground

Property value (BOOL)

TRUE: At runtime, the element is displayed in the foreground.

FALSE: At runtime, the element is displayed in the layer where it was inserted in the visualization editor.

See also

Element property 'Position'

The position defines the location and size of the element in the visualiza­tion window. These are based on the Cartesian coordinate system. The origin is located at the upper left corner of the window. The positive hori­zontal x-axis runs to the right. The positive vertical y-axis runs down­wards.

X

X coordinate of the upper left corner of the element

Specified in pixels.

Example: 10.

Y

Y coordinate of the upper left corner of the element

Specified in pixels.

Example: 10.

Width

Specified in pixels.

Example: 150

Height

Specified in pixels.

Example: 30

Note

You can also change the values by dragging the box symbols (_visu_icon_position_element.png) to other positions in the editor.

See also

Element property 'Background'

Background color

Drop-down list with background colors

Own image

  • image: Image ID of the background image.

    You select the background image from an image pool by clicking the button_threedots.png symbol.

    Info: If you specify the <default> value or select the image from the Default category in the input assistant, then the original element background image is used.

  • Transparent color: Selection from drop-down list or input assistant.

Optimized drawing

_cds_icon_option_activated.png: The background image is drawn one time. If there is a change in the foreground, then only the affected part of the image is redrawn.

_cds_icon_option_deactivated.png: The background image is redrawn in cycles.

Note: Deactivating this option is sensible only in certain exceptional cases.

Element property 'Arrow'

Hand style

Drop-down list with different arrow types

Color

  • _cds_icon_three_dots.png: The Color dialog box opens.

  • _cds_icon_arrow_down.png: Drop-down list with color names

Arrow start

Angle (in degrees) between the left edge of the element and the horizontal axis

Arrow end

Angle (in degrees) between the right edge of the element and the horizontal axis

Element property 'Scale'

Subscale position

  • Outside: The subscale is displayed on the outer scale ring (Frame outside).

  • Inside: The subscale is displayed on the inner scale ring (Frame inside).

Scale type

Type of scale

  • Lines

  • Dots

  • Squares

Scale start

Least value of the scale and the lower limit of the value range for the element.

Example: 0

_visu_icon_variable.png: The property Variable is shown below.

Variable

Variable (integer data type). Contains the scale start.

Example: PLC_PRG.iScaleStart

Declaration:

PROGRAM PLC_PRG VAR

iScaleStart : INT := 0;

END_VAR

Scale end

Greatest value of the scale and the upper limit of the value range for the element.

Example: 100

_visu_icon_variable.png: The property Variable is shown below.

Variable

Variable (integer data type). Contains the scale end.

Example: PLC_PRG.iScaleEnd

Declaration:

PROGRAM PLC_PRG VAR

iScaleEnd : INT := 120;

END_VAR

Main scale

Distance between two values on the rough scale.

Example: 10

_visu_icon_variable.png: The property Variable is shown below.

Variable

Variable (integer data type). Contains the distance.

Example: PLC_PRG.iMainScale

Declaration:

PROGRAM PLC_PRG VAR

iMainScale : INT := 20;

END_VAR

Subscale

Distance between two values on the fine scale.

You can hide the fine scale by setting the value to 0.

Example: 2

_visu_icon_variable.png: The property Variable is shown below.

Variable

Variable (integer data type). Contains the spacing.

Example: PLC_PRG.iSubScale

Declaration:

PROGRAM PLC_PRG VAR

iSubScale : INT := 5;

END_VAR

Scale line width

Specified in pixels.

Example: 3

Scale color

Color of scale lines

  • _cds_icon_three_dots.png: The Color dialog opens.

  • _cds_icon_arrow_down.png: A drop-down list with style colors opens.

Scale in 3D

_cds_icon_option_activated.png: Tick marks are displayed with slight 3D shadowing.

Note: This property is not displayed in FlatStyle.

Show scale

_cds_icon_option_activated.png: The scale is displayed.

Frame inside

_cds_icon_option_activated.png: A frame is drawn at the inner end of the scale.

Frame outside

_cds_icon_option_activated.png: A frame is drawn at the outer end of the scale.

Element property 'Label'

Label

Selection list

  • Outside: Scale values are placed outside of the scale.

  • Inside: Scale values are placed inside of the scale.

Unit

Text that is displayed in the element.

Example: Units displayed in m/s.

Font

Font for labels (example: scale numbering).

Selection from the drop-down list or by clicking the button. button_threedots.png

Scale format (C Syntax)

Values scaled in "printf" syntax

Examples: %d, %5.2f

Max. text width of labels

(optional) Value that redefines the maximum width of the scale label. The correct value is normally set automatically.

Note: Change this value only if the automatic adjustment does not yield the expected result.

Text height of labels

(optional) Value that redefines the maximum height of the scale label. The correct value is normally set automatically.

Note: Change this value only if the automatic adjustment does not yield the expected result.

Font color

Selection from the drop-down list or by clicking the button_threedots.png button.

Element property 'Positioning'

Usage of

  • Preset style values: Values from the current style

  • User-defined settings: The subnode Posi­tioning appears.

Positioning

Requirement: User-defined settings is selected as Usage of.

The displayed positioning settings depend on the type of needle instrument and potentiometer, and partially on whether a custom background image is selected. The following settings are used for achieving the exact position relative to the background image.

Needle movement

Length of the needle (in pixels)

Scale movement

Distance from the tick marks to the center (in pixels)

Requirement: A customer image is selected as Background.

Scale length

Length of the tick marks (in pixels)

Requirement: A customer image is selected as Background.

Label offset:

Distance from the labels to the tick marks (in pixels)

Unit offset:

Distance of the unit text Label ‣ Unit from the upper scale edge (in pixels)

Origin offset

Offset of the element (in pixels)

Requirement: For the elements Meter 180° and Meter 90°, this property is displayed only if a custom image is selected as Background.

Element property 'Colors'

Color areas

Durable color areas

_cds_icon_option_deactivated.png: All color areas are visible, regardless of the current value.

_cds_icon_option_activated.png: Only the color area is visible that includes the current value.

Use colors for scale

_cds_icon_option_activated.png: Colors in the color area are used only for the scale and frame.

Color areas

Create new

A new color area is added to the Elements view.

Delete

The color area is removed from the list and the list is refreshed.

Begin of area

Start value of the color area

Example: 20

_visu_icon_variable.png: The property Variable is shown below.

Variable

Variable (integer data type). Contains the start value.

Example: PLC_PRG.iColorAreaStart0

Declaration:

PROGRAM PLC_PRG VAR

iColorAreaStart0 : INT := 80;

END_VAR

End of area

End value of the color area

Example: 120

_visu_icon_variable.png: The property Variable is shown below.

Variable

Variable (integer data type). Contains the end value.

Example: iColorAreaEnd0

Declaration:

PROGRAM PLC_PRG VAR

iColorAreaEnd0 : INT := 100;

END_VAR

Color

Color that is used for displaying the area.

Element property 'State variables'

The variables control the element behavior dynamically.

Invisible

Variable (BOOL). Toggles the visibility of the element.

TRUE: The element is not visible at runtime.

Deactivate inputs

Variable (BOOL). Toggles the operability of the element.

TRUE: User inputs do not have any effect in runtime more. The element is shown as deactivated.

Note

The Invisible property is supported by the "Client Animation" functionality.

See also

Element property 'Absolute movement'

The properties contain IEC variables for controlling the position of the element dynamically. The reference point is the upper left corner of the element. In runtime mode, the entire element is moved.

Movement

X

Variable (numeric data type). Defines the X position (in pixels).

Example: PLC_PRG.iPos_X.

Increasing this value in runtime mode moves the element to the right.

Y

Variable (numeric data type). Defines the Y position (in pixels).

Example: PLC_PRG.iPos_Y.

Increasing this value in runtime mode moves the element downwards.

Rotation

Variable (numeric data type). Defines the angle of rotation (in degrees).

Example: PLC_PRG.iAngle1.

The midpoint of the element rotates at the Center point. This rotation point is shown as the _visu_icon_center_point.png symbol.

In runtime mode, the alignment of the element remains the same with respect to the coordinate system of the visualization. Increasing the value rotates the element to the right.

_visu_img_prp_rotation.png 

Interior rotation

Variable (numeric data type). Defines the angle of rotation (in degrees).

Example: PLC_PRG.iAngle2.

In runtime mode, the element rotates about the point of rotation specified in Center according to the value of the variable. In addition, the alignment of the element rotates according to the coordinate system of the visualization. Increasing the value in the code rotates clockwise.

The rotation point is shown as the _visu_icon_center_point.png symbol.

Note: If a static angle of rotation is specified in the Position ‣ Angle property, then the static angle of rotation is added to the variable angle of rotation (offset) when the visualization is executed.

_visu_img_prp_inner_rotation.png 

Note

You can link the variables to a unit conversion.

Note

The X, Y, Rotation, and Interior rotation properties are supported by the "Client Animation" functionality.

See also

Element property 'Access rights'

Requirement: User management is set up for the visualization.

Access rights

Opens the Access rights dialog. There you can edit the access privileges for the element.

Status messages:

  • Not set. Full rights.: Access rights for all user groups : operable

  • Rights are set: Limited rights: Access is restricted for at least one group.

See also