Visualization Element 'Time range picker'
Tag: Date/time controls
The element provides configurable buttons for setting the time range of a trend display to a defined time. In the process the end time of the previous display is left unchanged and the start time is adapted.
Element name |
Optional Hint: Assign individual names for elements so that they are found faster in the element list. Example: TimeRangeTemperature |
Type of element |
Time range picker |
The position defines the location and size of the element in the visualization window. These are based on the Cartesian coordinate system. The origin is located at the upper left corner of the window. The positive horizontal x-axis runs to the right. The positive vertical y-axis runs downwards.
X |
X coordinate of the upper left corner of the element Specified in pixels. Example: 10. |
Y |
Y coordinate of the upper left corner of the element Specified in pixels. Example: 10. |
Width |
Specified in pixels. Example: 150 |
Height |
Specified in pixels. Example: 30 |
Note
You can also change the values by dragging the box symbols () to other positions in the editor.
See also
Orientation |
Specifies whether the time picker element is aligned horizontally or vertically in the editor. Hint: Change the width to height ratio of the element in the editor. |
Show frame |
|
Resolution |
Resolution saved for the time stamp: Millisecond or Microsecond |
Attached element instance |
Assignment to the element that processes the time picker Example: GenElemInst_1
Hint: Click the |
Text |
String label for the element. Example: Zoom |
Element property 'Text properties'
The properties contain fixed values for the text properties.
Font |
Example: Default
|
Font color |
Example: Black
|
Transparency |
Whole number (value range from 0 to 255). This determines the transparency of the respective color. Example: 255: The color is opaque. 0: The color is completely transparent. Please note: If the color is a style color and already has a transparency value, then this property is write-protected. |
In Times, the buttons that the element provides at runtime are defined and configured in an array.
Provide "All" selection |
|
Times |
|
Times
with index ∈ {0, 1, 2,...} |
Array of all buttons in the time selection bar. Index corresponds to the number of buttons.
|
[Index]
|
|
Element property 'Control variables'
Time |
Displays which time is currently selected. Variable (STRING) Example: PLC_PRG.strSelcetedTime |
"All" selected |
Displays the state of the "All" button Variable (BOOL) Example: PLC_PRG.AllTimesAreSelected |
Control variables |
The element is displayed horizontally or vertically depending on the width/height ratio. |
Show frame |
|
Resolution |
Resolution saved for the time stamp: Millisecond or Microsecond |
Attached element instance |
Requirement:
The element can be assigned to a Trend visualization element. In this way, the time range of the trend element can be changed. The available visual elements are selected with the help of the input assistance ( |
Element property 'Absolute movement'
The properties contain IEC variables for controlling the position of the element dynamically. The reference point is the upper left corner of the element. In runtime mode, the entire element is moved.
Movement |
||
X |
Variable (numeric data type). Defines the X position (in pixels). Example: PLC_PRG.iPos_X. Increasing this value in runtime mode moves the element to the right. |
|
Y |
Variable (numeric data type). Defines the Y position (in pixels). Example: PLC_PRG.iPos_Y. Increasing this value in runtime mode moves the element downwards. |
|
Rotation |
Variable (numeric data type). Defines the angle of rotation (in degrees). Example: PLC_PRG.iAngle1.
The midpoint of the element rotates at the Center point. This rotation point is shown as the In runtime mode, the alignment of the element remains the same with respect to the coordinate system of the visualization. Increasing the value rotates the element to the right. |
|
Interior rotation |
Variable (numeric data type). Defines the angle of rotation (in degrees). Example: PLC_PRG.iAngle2. In runtime mode, the element rotates about the point of rotation specified in Center according to the value of the variable. In addition, the alignment of the element rotates according to the coordinate system of the visualization. Increasing the value in the code rotates clockwise.
The rotation point is shown as the Note: If a static angle of rotation is specified in the Position ‣ Angle property, then the static angle of rotation is added to the variable angle of rotation (offset) when the visualization is executed. |
|
Note
You can link the variables to a unit conversion.
Note
The X, Y, Rotation, and Interior rotation properties are supported by the "Client Animation" functionality.
See also
Element property 'State variables'
The variables control the element behavior dynamically.
Invisible |
Variable (BOOL). Toggles the visibility of the element. TRUE: The element is not visible at runtime. |
Note
The Invisible property is supported by the "Client Animation" functionality.
See also
These properties are available only when you select the Preview: Support client animations and overlay of native elements option in the Visualization Manager.
You can animate a movement, a rotation, and the visibility of a visualization element.
Animation time |
Time that the element executes an animation (in milliseconds) Example: 500 |
Move to the foreground |
Property value (BOOL) TRUE: At runtime, the element is displayed in the foreground. FALSE: At runtime, the element is displayed in the layer where it was inserted in the visualization editor. |
See also
Element property 'Access rights'
Requirement: User management is set up for the visualization.
Access rights |
Opens the Access rights dialog. There you can edit the access privileges for the element. Status messages:
|
See also