Visualization Element 'Cartesian XY Chart'
Tag: Special controls
The element displays the curve of array values graphically as a line or bar chart in the Cartesian coordinate system. The chart can display multiple curves at one time.
Notice
Restriction The element can be used with controller with V3.5 SP11 and later.
Note
In the CODESYS Store, you will find a sample project for using XY chart elements in visualizations.
|
Element name |
Example: Velocity chart |
|
Type of element |
XY Chart |
|
Cartesian XY Chart |
|
The position defines the location and size of the element in the visualization window. These are based on the Cartesian coordinate system. The origin is located at the upper left corner of the window. The positive horizontal x-axis runs to the right. The positive vertical y-axis runs downwards.
|
X |
X coordinate of the upper left corner of the element Specified in pixels. Example: 10. |
|
Y |
Y coordinate of the upper left corner of the element Specified in pixels. Example: 10. |
|
Width |
Specified in pixels. Example: 150 |
|
Height |
Specified in pixels. Example: 30 |
Note
You can also change the values by dragging the box symbols (
) to other positions in the editor.
See also
Element property 'Element look'
The properties contain fixed values for defining the look of the element.
|
Border line width |
Value in pixels Example: 2 Note: The values 0 and 1 both result in a line weight of one pixel. If no line should be displayed, then the Border line style property must be set to the option Invisible. |
|
Border line style |
|
|
Frame line color |
|
|
Font |
Example: Default
|
Element property 'Control variables'
|
Zooming the displayed curve is done by means of the mouse, or the pinch gesture on a multitouch device. It also applies to all axes. At runtime when Enable is TRUE, you can draw a box with the mouse by holding down the left mouse button. When you release the mouse button, the display zooms in on the box and the curve is magnified. To zoom in and out on a multitouch device, move two fingers together or away from each other, respectively. Zooming and panning can work together. |
|
|
Enable |
Variable (BOOL) that enables or disables zooming. TRUE: Enables zooming Example: PLC_PRG.xZoomEnable |
|
Home |
Variable (BOOL). Rising edge: Reset the displayed curve to the initial state after the display has changed due to zooming. Example: PLC_PRG.xZoomHome |
|
Undo |
Variable (BOOL). Rising edge: Reset the displayed curve to the previous position after the display has changed due to zooming. Example: PLC_PRG.xZoomUndo |
|
Is zoomed |
Variable (BOOL) that indicates whether or not the displayed curve was modified due to zooming. TRUE: Curve setting was zoomed. Example: PLC_PRG.xIsZoomed |
|
Panning the displayed curve is done by means of the mouse or the pinch gesture on a multitouch device. It also applies to all axes. At runtime if Enable is TRUE, then you can drag the displayed curve to another position by holding down the left mouse button. To pan the displayed curve on a multitouch device, drag it with one finger to another position. |
|
|
Enable |
Variable (BOOL) to enable or disable panning. TRUE: Enables panning Example: PLC_PRG.xPanEnable |
|
Home |
Variable (BOOL). Rising edge: Reset the displayed curve to the initial position after the display has changed due to panning. Example: PLC_PRG.xPanHome |
|
Is panned |
Variable (BOOL) whose state indicates whether or not the displayed curve was modified due to zooming. TRUE: Curve setting was panned. Example: PLC_PRG.xIsPanned |
Element property 'Absolute movement'
The properties contain IEC variables for controlling the position of the element dynamically. The reference point is the upper left corner of the element. In runtime mode, the entire element is moved.
|
Movement |
||
|
X |
Variable (numeric data type). Defines the X position (in pixels). Example: PLC_PRG.iPos_X. Increasing this value in runtime mode moves the element to the right. |
|
|
Y |
Variable (numeric data type). Defines the Y position (in pixels). Example: PLC_PRG.iPos_Y. Increasing this value in runtime mode moves the element downwards. |
|
|
Rotation |
Variable (numeric data type). Defines the angle of rotation (in degrees). Example: PLC_PRG.iAngle1.
The midpoint of the element rotates at the Center point. This rotation point is shown as the In runtime mode, the alignment of the element remains the same with respect to the coordinate system of the visualization. Increasing the value rotates the element to the right. |
|
|
Interior rotation |
Variable (numeric data type). Defines the angle of rotation (in degrees). Example: PLC_PRG.iAngle2. In runtime mode, the element rotates about the point of rotation specified in Center according to the value of the variable. In addition, the alignment of the element rotates according to the coordinate system of the visualization. Increasing the value in the code rotates clockwise.
The rotation point is shown as the Note: If a static angle of rotation is specified in the Position ‣ Angle property, then the static angle of rotation is added to the variable angle of rotation (offset) when the visualization is executed. |
|
Note
You can link the variables to a unit conversion.
Note
The X, Y, Rotation, and Interior rotation properties are supported by the "Client Animation" functionality.
See also
Element property 'State variables'
The variables control the element behavior dynamically.
|
Invisible |
Variable (BOOL). Toggles the visibility of the element. TRUE: The element is not visible at runtime. |
|
Deactivate inputs |
Variable (BOOL). Toggles the operability of the element. TRUE: User inputs do not have any effect in runtime more. The element is shown as deactivated. |
Note
The Invisible property is supported by the "Client Animation" functionality.
See also
These properties are available only when you select the Preview: Support client animations and overlay of native elements option in the Visualization Manager.
You can animate a movement, a rotation, and the visibility of a visualization element.
|
Animation time |
Time that the element executes an animation (in milliseconds) Example: 500 |
|
Move to the foreground |
Property value (BOOL) TRUE: At runtime, the element is displayed in the foreground. FALSE: At runtime, the element is displayed in the layer where it was inserted in the visualization editor. |
See also
Element property 'Access rights'
Requirement: User management is set up for the visualization.
|
Access rights |
Opens the Access rights dialog. There you can edit the access privileges for the element. Status messages:
|
See also