How to Change Variable Values via the Visualization

 

In addition to displaying values from the controller, a user interface is also used to enter and change values.

In general, you can configure user input for each element in its Input­configuration properties. Moreover, elements have been developed especially for specific input.

Examples:

See also