You can capture user input events in the application. For this purpose, you can implement a function block that is executed when user events occur.
Capturing the writing of variables
When the user completes the input of a value (in an input field), an edit control event is closed. You can capture this event in the application as follows.
Create a function block that implements the VisuElems.IEditBoxInputHandler interface from the VisuElemBase library.
Pass the instance to the global event manager VisuElems.Visu_Globals.g_VisuEventManager by calling the SetEditBoxEventHandler method.
Example
A visualization has two input fields for iInput_A and rInput_B and one text output element.
The input fields are rectangles that the user is prompted to click in order to input text.
The text output element is a rectangle where the contents of the text variable PLC_PRG.stInfo are printed. The text variable contains the last input by a user in one of the input fields and the additional information that was added.
|
Properties of the rectangle iInput_A |
|
|
Texts ‣ Text |
iInput_A: %i |
|
Text variables ‣ Text variable |
PLC_PRG.iInput_A |
|
Properties of the rectangle rInput_B |
|
|
Texts ‣ Text |
iInput_B: %i |
|
Text variables ‣ Text variable |
PLC_PRG.rInput_B |
|
Properties of the rectangle for the text output |
|
|
Texts ‣ Text |
%s |
|
Text variables ‣ Text variable |
PLC_PRG.stInfo |
PLC_PRG implementation
PROGRAM PLC_PRG
VAR_INPUT
iInput_A:INT; (* Used in the visualization as user input variable*)
rInput_B:REAL; (* Used in the visualization as user input variable*)
stInfo : STRING; (* Informs about the user input via the edit control field;
String gets composed by method 'VariableWritten;
Result is displayed in the lower rectangle of the visualization *)
END_VAR
VAR
inst : POU;
bFirst : BOOL := TRUE;
END_VAR
IF bFirst THEN
bFirst := FALSE;
VisuElems.Visu_Globals.g_VisuEventManager.SetEditBoxEventHandler(inst);
(* Call of method VariableWritten *)
END_IF
POU implementation
FUNCTION_BLOCK POU IMPLEMENTS VisuElems.IEditBoxInputHandler
(* no further declarations, no implementation code *)
Method VariableWritten assigned to POU
METHOD VariableWritten : BOOL
(* provides some information always when an edit control field is closed in the visualization, that is a variable gets written by user input in one of the upper rectangles *)
VAR_INPUT
pVar : POINTER TO BYTE;
varType : VisuElems.Visu_Types;
iMaxSize : INT;
pClient : POINTER TO VisuElems.VisuStructClientData;
END_VAR
// String stInfo, which will be displayed in the lower rectangle, is composed here
PLC_PRG.stInfo := 'Variable written; type: ';
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, INT_TO_STRING(varType));
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, ', adr: ');
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, DWORD_TO_STRING(pVar));
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, ', by: ');
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, SEL(pClient^.globaldata.clienttype = VisuElems.Visu_ClientType.Targetvisualization,'other visu', 'targetvisu'));
When the user presses and releases the key, a keyboard event is triggered in the visualization. You can capture this event in the application as follows.
Create a function block that implements VisuElems.IVisuUserEventManager from the VisuElemBase library.
Pass the instance to the global event manager VisuElems.Visu_Globals.g_VisuEventManager by calling the SetKeyEventHandler method.
Example
A visualization has one text output element. The text output element is a rectangle where the contents of the text variable PLC_PRG.stInfo are printed. The text variable contains information about the last key pressed by the user.
|
Properties of the rectangle for the text output |
|
|
Texts ‣ Text |
%s |
|
Text variables ‣ Text variable |
PLC_PRG.stInfo |
Implementation of the PLC_PRG program
PROGRAM PLC_PRG
VAR_INPUT
stInfo : STRING;
END_VAR
VAR
inst : POU;
bFirst : BOOL := TRUE;
END_VAR
IF bFirst THEN
bFirst := FALSE;
VisuElems.Visu_Globals.g_VisuEventManager.SetKeyEventHandler(inst);
END_IF
Implementation of the POU function block
FUNCTION_BLOCK POU IMPLEMENTS VisuElems.IKeyEventHandler
(* no further declarations, no implementation code *)
Implementation of the VariableWritten method of the POU function block
/// This method will be called after a key event is released.
/// RETURN:
/// TRUE - When the handler has handled this event and it should not be handled by someone else
/// FALSE - When the event is not handled by this handler
METHOD HandleKeyEvent : BOOL
VAR_INPUT
/// Event type. The value is true if a key-up event was released.
bKeyUpEvent : BOOL;
/// Key code
dwKey : DWORD;
/// Modifier. Possible values:
/// VISU_KEYMOD_SHIFT : DWORD := 1;
/// VISU_KEYMOD_ALT : DWORD := 2;
/// VISU_KEYMOD_CTRL : DWORD := 4;
dwModifiers : DWORD;
/// Pointer to the client structure were the event was released
pClient : POINTER TO VisuStructClientData;
END_VAR
VAR
END_VAR
PLC_PRG.stInfo := 'KeyEvent up: ';
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, BOOL_TO_STRING(bKeyUpEvent));
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, ', key: ');
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, DWORD_TO_STRING(dwKey));
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, ', modifier: ');
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, DWORD_TO_STRING(dwModifiers));
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, ', by: ');
PLC_PRG.stInfo := CONCAT(PLC_PRG.stInfo, SEL(pClient^.globaldata.clienttype =
VisuElems.Visu_ClientType.Targetvisualization,
'other visu', 'targetvisu'));
Recording variable value changes triggered by input events
All visualization elements that change the value of a variable by user input call the IValueChangedListener interface. With this interface, the value changes can be recorded and then processed programmatically.
Note
In CODESYS Store, you will find the sample project "Visu Value Change Handler". The sample project records variable value changes that were triggered by user input within the visualization. In this project. you will also find the implementation of the ValueChanged method.
Implement a function block (example: POU) that implements the IValueChangedListener interface.
FUNCTION_BLOCK POU IMPLEMENTS VisuElems.IValueChangedListener
⇒ In the device tree, the ValueChanged method is inserted below the function block.
In a program (example: PLC_PRG), implement the IEC code that registers the interface.
VisuElems.g_itfValueChangedListenerManager.AddValueChangedListener(itfValueChangedListener)
⇒ PLC_PRG receives all value changes by means of the ValueChanged method.
Now you can record and process the value changes.