Placeholders with Format Definition in the Output Text
A character string that is output in the visualization can include the placeholder % for a variable. At runtime, the placeholder is replaced by the actual value of the variable in the defined format. The data type in the format definition and of the variable must be identical. A character string can contain a maximum of one placeholder.
Character strings for output are listed in the Text property. The associated variable is listed in the Text variable property.
See also
|
%d %i |
Printing a variable (integer data type) as a decimal number |
Code: iCounter : INT := 12; Property Text: Value: %i Property Text variable: PLC_PRG.iCounter Output: Value: 12 |
|
%b |
Printing a variable (integer data type) as a binary number |
Code: byCode : BYTE := 255; Property Text: Coding: %b Property Text variable: PLC_PRG.byCode Output: Coding: 11111111 |
|
%o |
Printing a variable (integer data type) as an unsigned octal number without a preceding zero |
Code: byCode : BYTE := 8#377; Property Text: Coding: %o Property Text variable: PLC_PRG.byCode Output: Coding: 377 |
|
%x |
Printing a variable (integer data type with maximum 32 bits) as an unsigned hexadecimal number without a preceding "0x" |
Code: dwCode : INT := 16#FFFFFFFF; Property Text: Coding: %x Property Text variable: PLC_PRG.dwCode Output: Coding: ffffffff |
|
%llX %012llX |
Output of a 64-bit variable (LWORD, LINT, ULINT) as a hexadecimal number. Note: llx means "long long hexadecimal" |
Code: lwCode : LWORD := 16#4FFF_3FFF_2FFF_1FFF; Property Text: Coding: %llx Property Text variable: PLC_PRG.lwCode Output: Coding: 4fff3fff2fff1fff |
|
%u |
Printing a variable (integer data type) as an unsigned decimal number |
Code: uiNumber : UINT := 1234; Property Text: Number: %u Property Text variable: PLC_PRG.uiNumber Output: Number: 1234 |
Printing floating-point numbers
Floating-point numbers have the data type REAL or LREAL.
|
%f |
In decimal form with decimal point in format 1.6 |
Code: rWeight : REAL := 1.123456789; Property Text: Weight: %f Property Text variable: PLC_PRG.rWeight Output: Weight: 1.123456 |
|
%<alignment><minimum width>.<accuracy>f |
As decimal number in user-defined format
|
Code: rWeight : REAL := 12.1 Property Text: Weight: %2.3f Property Text variable: PLC_PRG.rWeight Output: Weight: 12,100 |
|
%e |
Printing a floating-point number (REAL or LREAL) in exponential notation of base 10 |
Code: rValue : REAL := 1.234567%e-003; Property Text: Value: %E Property Text variable: PLC_PRG.rValue Output: Value: 1.23E-6 |
|
%E |
Code: rValue : REAL := 1.234567%e-003; Property Text: Value: %e Property Text variable: PLC_PRG.rValue Output: Value: 1.23e-6 |
|
%c |
Printing a single character in ASCII |
Code: bChar := 16#41; Property Text: Key: %c PropertyText variable: PLC_PRG.bChar Output: Key: A |
|
%s |
Printing a character string |
Code: strName := 'Paul Smith'; Property Text: Name: %s Property Text variable: PLC_PRG.strName Output: Name: Paul Smith |
|
%% |
Printing the percent sign in a character string |
Property Text: Valid until 90%% Output: Valid until 90% |
|
Code: iPercentage : INT := 80; Property Text: Valid until %d%%. Property Text variable: PLC_PRG.iPercentage := 80; Output: Valid until 80% |
If the output text in the element property Text contains the placeholder "%t", then a date and/or time is printed. If a variable is not specified in the property Text variable, then the system time is printed; otherwise it is the value of the variable.
The names of the days and months are displayed in English by default. If localized texts are used, then the text list System has to be supplemented. This text list is created automatically in the POUs view when the placeholder %t is used. The English terms have to be used as the ID here. The localization can be done for both the abbreviated and full names.
Time data types include LTIME, TIME, TIME_OF_DAY, TOD, DATE, DATE_AND_TIME, and DT.
|
Date and time formats |
||
|
%t[yyyy] |
Years with century (4 digits) |
Code: dateBy : DATE := DATE#2020-1-1; Property Text: By the year %t[yyyy] Property Text variable: PLC_PRG.dateBy Output: By the year 2020 |
|
%t[yy] |
Years without century (00-99) |
Code: dateSince : DATE := DATE#2000-1-1; Property Text: Since: %t[yy] Property Text variable: PLC_PRG.dateSince Output: Since: 00 |
|
%t[y] |
Years without century (0-99) |
Code: dateSince : DATE := DATE#2000-1-1; Property Text: Since: %t[y] Property Text variable: PLC_PRG.dateSince Output: Since: 0 |
|
%t[MMMM] |
Months as a full name |
Code: dateMonth : DATE := DATE#2016-1-1; Property Text: Month: %t[MMMM] Property Text variable: PLC_PRG.dateMonth Output: Month: January |
|
%t[MMM] |
Months as an abbreviated name |
Code: dateMonth : DATE := DATE#2016-1-1; Property Text:: Month: %t[MMM] Property Text variable: PLC_PRG.dateMonth Output: Month: Jan |
|
%t[MM] |
Months as a number (01 – 12) |
Code: dateMonth : DATE := DATE#2016-1-1; Property Text:: Month: %t[MM] Property Text variable: PLC_PRG.dateMonth Output: Month: 01 |
|
%t[M] |
Months as a number (1 – 12) |
Code: dateMonth : DATE := DATE#2016-1-1; Property Text:: Month: %t[M] Property Text variable: PLC_PRG.dateMonth Output: Month: 1 |
|
%t[ddddd] |
Days of week as a number (1=Monday to 7=Sunday) |
Code: iDay : INT := 7; Property Text:: Day: %t[ddddd] Property Text variable: PLC_PRG.iDay Output: Day: 7 |
|
%t[dddd] |
Days of week as a full name |
Code: iDay : INT := 7; Property Text:: Day: %t[dddd] Property Text variable: PLC_PRG.iDay Output: Day: Sunday |
|
%t[ddd] |
Days of week as an abbreviated name |
Code: iDay : INT := 7; Property Text:: Day: %t[ddd] Property Text variable: PLC_PRG.iDay Output: Day: Sun |
|
%t[dd] |
Days in month as a number (01 – 31) |
Code: iDay : INT := 1; Property Text:: Day: %t[dd] Property Text variable: PLC_PRG.iDay Output: Day: 01 |
|
%t[d] |
Days in month as a number (1 – 31) |
Code: iDay : INT := 1; Property Text:: Day: %t[d] Property Text variable: PLC_PRG.iDay Output: Day: 1 |
|
%t[jjj] |
Days in year as a number (001-366) |
Code: dateOfNoReturn : DATE := DATE#2016-09-01; Property Text:: Day of no return: %t[jjj] Property Text variable: PLC_PRG.dateOfNoReturn Output: Day of no return: 245 |
|
%t[HH] |
Hours in 24-hour format (00-23) |
Code: todEnd : TOD := TIME_OF_DAY#17:0:0; Property Text: Ends at: %t[HH]:00 Property Text variable: PLC_PRG.todEnd Output: Ends at 17:00 |
|
%t[hh] |
Hours in 12-hour format (01-12) |
Code: todEnd : TOD := TIME_OF_DAY#17:0:0; Property Text: Ends at: %t[hh]:00 o'clock Property Text variable: PLC_PRG.todEnd Output: Ends at 17:00 o'clock |
|
%t[mm] |
Minutes with leading zeros (00-59) |
Code: tPeriod : TIME := T#5M; Property Text: Period: %t[mm]m Property Text variable: PLC_PRG.tPeriod Output: Period: 05m |
|
%t[m] |
Minutes without leading zeros (0-59) |
Code: tPeriod : TIME := T#5m; Property Text: Period: %t[m 'm'] Property Text variable: PLC_PRG.tPeriod Output: Period: 5 m |
|
%t[ss] |
Seconds with leading zeros (00-59) |
Code: tPeriod : TIME := T#5m3s; Property Text: Period: %t[mm'm'ss's'] Property Text variable: PLC_PRG.tPeriod Output: Period: 05m03s |
|
%t[s] |
Seconds without leading zeros (0-59) |
Code: tPeriod : TIME := T#5m3s; Property Text: Period: %t[m'm's's'] Property Text variable: PLC_PRG.tPeriod Output: Period: 5m3s |
|
%t[ms] |
Milliseconds without leading zeros (0-999) |
Code: tPeriod : TIME := T#500ms; Property Text: Period: %t[ms'ms'] Property Text variable: PLC_PRG.tPeriod Output: Period: 500ms |
|
%t[us] |
For LTIME variables only: microsecond definition (0-999) |
Code: ltPeriod :LTIME := LTIME#1000D23H44M12S34MS2US44NS; Property Text: 'Period': %t[dd.HH.m.s.ms.us.ns] Property Text variable: PLC_PRG.ltPeriod Output: Period: 1000.23.44.12.34.2.44 Hint: Overflow is permitted in the greatest time unit of a definition. |
|
%t[ns] |
For LTIME variables only: nanosecond definition (0-999) |
|
|
%t[t] |
If the value is a time < 12h, then A is printed; otherwise P is printed. |
Code: tClosed : TOD := TOD#17:17:17.17; Property Text: Closed at %t[hht] Property Text variable: PLC_PRG.tClosed Output: Closed at 5P |
|
%t[tt] |
If the value is a time < 12h, then AM is printed; otherwise PM is printed. |
Code: tClosed : TOD := TOD#17:17:17.17; Property Text: Closed at %t[hh tt] Property Text variable: PLC_PRG.tClosed Output: Closed at 5 PM |
|
%t[' '] |
If character strings should be printed that correspond to a format definition, then these must be represented in single straight quotation marks. |
|
|
The format definitions can be represented in a series. |
||
|
%t[HH:mm:ss:ms] |
Printing the complete time |
Code: dwTime : DWORD := 4294967295; Property Text: Time: %t[HH:mm:ss:ms] Property Text variable: PLC_PRG.dwTime Output: Time: 23:59:59:999 |
|
%t[yyyy-MM-dd dddd] |
Printing the date and day of the week |
Code: dateSet : DATE := DATE#2016-02-12; Property Text: Date: %t[yyyy-MM-dd dddd] Property Text variable: PLC_PRG.dateSet Output: Date: 2016-02-12 Friday |