Displaying Data Curve with Trend

 

A trend visualizes data that is used in the database of a trend recording. In contrast to the trace element, the trend element is particularly appro­priate for long-term data recording.

_visu_img_trend.png

The visualization of a trend encompasses the Trend element and the control elements. The three possible control elements can be seen in the illustration.

A cursor is optionally available that enables the reading of a value at a certain time.

You can display a trend visualization in the following variants:

See also