Displaying Data Arrays in Tables
A frequently required function of a user interface is the display of data arrays. CODESYS Visualization provides the element Table for this.
In the configuration of the element Table, enter an array variable in the property Data array. The array components are displayed in the rows and columns of the table.
A table for displaying data arrays can also be created in the following way. You duplicate a single element having at least one property that is described by a structured variable. The single element is configured as a "template" for this and duplicated with a command.