EcoStruxure Machine Expert version 1.1 does not support the M258, LMC058 and LMC078 controllers.

Example Description

 

Overview

Short Description

The project implements an application example which shows how to implement email handling in a controller application using the EmailHandling library.

System Requirements and Limitations

The application example has been created and tested with, or supported by, the components listed in the table:

Component

Type and Version

Software

oEcoStruxure Machine Expert V1.1

Controller

oModicon M241 Logic Controller1)

oModicon M251 Logic Controller

oModicon M258 Logic Controller1)

oModicon LMC058 Motion Controller1)

oModicon M262 Logic/Motion Controller

oPacDrive LMC 1xx / 2xx1)

oPacDrive LMX 300 / 4xx/ 600 / 802C1)

Additional devices

A PC with a running Email server and an additional Email client.

Additional requirements

The Email server is running on a PC and can be reached from the controller through the network.

1)   The concepts presented in the application example are in principle, transferable to other controllers supporting the controller firmware released in conjunction with EcoStruxure Machine Expert V1.1.