How to Change the IP Address of the Controller
changeIPAddress: Change the IP address of the controller
The changeIPAddress function block provides the capability to change dynamically a controller IP address, its subnet mask and its gateway address. The function block can also save the IP address so that it is used in subsequent reboots of the controller.
NOTE: Changing the IP addresses is only possible if the IP mode is configured to fixed IP address. For more details, refer to IP Address Configuration.
NOTE: For more information on the function block, use the Documentation tab of EcoStruxure Machine Expert Library Manager Editor. For the use of this editor, refer EcoStruxure Machine Expert Programming Guide.
Input |
Type |
Comment |
---|---|---|
xExecute |
BOOL |
oRising edge: action starts. oFalling edge: resets outputs. If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event that an error is detected. In this case, the corresponding output values (xDone, xError, iError) are present at the outputs for exactly one cycle. |
xSave |
BOOL |
TRUE: save configuration for subsequent reboots of the controller. |
eChannel |
changeIPAddress_Channel |
The input eChannel is the Ethernet port to be configured. Depending on the number of the ports available on the controller, it is one of 5 values in changeIPAddress_Channel (0 or 1). |
i_abyIPAddress |
ARRAY[0..3] OF BYTE |
The new IP Address to be configured. Format: 0.0.0.0. NOTE: If this input is set to 0.0.0.0 then the controller default IP addresses is configured. |
i_abyIPMask |
ARRAY[0..3] OF BYTE |
The new subnet mask. Format: 0.0.0.0 |
i_abyIPGateway |
ARRAY[0..3] OF BYTE |
The new gateway IP address. Format: 0.0.0.0 |
Output |
Type |
Comment |
---|---|---|
xDone |
BOOL |
TRUE: if IP Addresses have been successfully configured or if default IP Addresses have been successfully configured because input i_abyIPAddress is set to 0.0.0.0. |
xBusy |
BOOL |
Function block active. |
xError |
BOOL |
oTRUE: error detected, function block aborts action. oFALSE: no error has been detected. |
eError |
changeIPAddress_Error |
|
xSaved |
BOOL |
Configuration saved for the subsequent reboots of the controller. |
q_abyIPAddress |
ARRAY[0..3] OF BYTE |
Current controller IP address. Format: 0.0.0.0. |
q_abyIPMask |
ARRAY[0..3] OF BYTE |
Current subnet mask. Format: 0.0.0.0. |
q_abyIPGateway |
ARRAY[0..3] OF BYTE |
Current gateway IP address. Format: 0.0.0.0. |
changeIPAddress_Channel: Ethernet port to be configured
The changeIPAddress_Channel enumeration data type contains the following values:
Enumerator |
Value |
Description |
---|---|---|
CHANNEL_ETHERNET_NETWORK |
0 |
M241, M251MESC, M258, LMC058, LMC078: Ethernet port M251MESE: Ethernet_2 port |
CHANNEL_DEVICE_NETWORK |
1 |
M241: TM4ES4 Ethernet port M251MESE: Ethernet_1 port |
CHANNEL_M262_ETH1 |
2 |
Ethernet_1 port |
CHANNEL_M262_ETH2 |
3 |
Ethernet_2 port |
CHANNEL_M262_TMS1 |
4 |
1st TMS module |
changeIPAddress_Error: Error Codes
The changeIPAddress_Error enumeration data type contains the following values:
Enumerator |
Value |
Description |
---|---|---|
ERR_NO_ERROR |
00 hex |
No error detected. |
ERR_UNKNOWN |
01 hex |
Internal error detected. |
ERR_INVALID_MODE |
02 hex |
IP address is not configured as a fixed IP address. |
ERR_INVALID_IP |
03 hex |
Invalid IP address. |
ERR_DUPLICATE_IP |
04 hex |
The new IP address is already used in the network. |
ERR_WRONG_CHANNEL |
05 hex |
Incorrect Ethernet communication port. |
ERR_IP_BEING_SET |
06 hex |
IP address is already being changed. |
ERR_SAVING |
07 hex |
IP addresses not saved due to a detected error or no non-volatile memory present. |
ERR_DHCP_SERVER |
08 hex |
A DHCP server is configured on this Ethernet communication port. |