About the Book

At a Glance

The EcoStruxure Machine Expert - Safety application software is used to develop the Safety Logic Controller system.

Validity Note

The present document has been updated with the release of EcoStruxure Machine Expert - Safety V1.1.

The technical characteristics of the devices described in this document also appear online. To access this information online:

Step

Action

1

Go to the Schneider Electric home page www.schneider-electric.com.

2

In the Search box type the reference of a product or the name of a product range.

  • Do not include blank spaces in the reference or product range.

  • To get information on grouping similar modules, use aster­isks (*).

3

If you entered a reference, go to the Product Datasheets search results and click on the reference that interests you.

If you entered the name of a product range, go to the Product Ranges search results and click on the product range that inter­ests you.

4

If more than one reference appears in the Products search results, click on the reference that interests you.

5

Depending on the size of your screen, you may need to scroll down to see the data sheet.

6

To save or print a data sheet as a .pdf file, click Download XXX product datasheet.

Title of Documentation

Reference Number

Modicon TM5 Safety Logic Controller SLC100/200 FS Hardware Guide

EIO0000000889 (Eng)

Modicon TM5/TM7 Digital I/O Safety Modules Hardware Guide

EIO0000000861 (Eng),

EIO0000000862 (Ger),

EIO0000000863 (Fre),

EIO0000000864 (Ita),

EIO0000000865 (Spa),

EIO0000000866 (Chs)

Modicon TM7 Digital I/O Modules Hardware Guide

EIO0000000703 (Eng),

EIO0000000704 (Fre),

EIO0000000705 (Ger),

EIO0000000706 (Spa),

EIO0000000707 (Ita),

EIO0000000704 (Chs)

TM5SD••• Instruction Sheet

S1A85744

TM7SDM12DTFS Instruction Sheet

S1A85745

TM5CSLC• /TM5ACSLCM•• Instruction Sheet

S1A85742

LMC Pro/Pro2 Hardware Guide

EIO0000001503 (Eng)

EIO0000001504 (Ger)

Operating Manual TM5 SERCOS III Bus Interface

www.elau.com

PacDrive TM5/TM7 Flexible Safety System - System Planning and Installation Guide

EIO0000001064 (Eng),

EIO0000001066 (Ger),

XY2AU1 / XY2AU1 Instruction Sheet

163437801A55 (EN, DE, PT, ES, IT, FR)

SlcRemoteController library guide

EIO0000002149 (Eng),

EIO0000002150 (Ger),

You can download these technical publications and other technical infor­mation from our website at www.schneider-electric.com.

Product Related Information

WARNING

LOSS OF CONTROL

  • The designer of any control scheme must consider the potential failure modes of control paths and, for certain critical control func­tions, provide a means to achieve a safe state during and after a path failure. Examples of critical control functions are emergency stop and overtravel stop, power outage and restart.

  • Separate or redundant control paths must be provided for critical control functions.

  • System control paths may include communication links. Consider­ation must be given to the implications of unanticipated transmis­sion delays or failures of the link.

  • Observe all accident prevention regulations and local safety guide­lines.1

  • Each implementation of this equipment must be individually and thoroughly tested for proper operation before being placed into service.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

1

For additional information, refer to NEMA ICS 1.1 (latest edition), "Safety Guidelines for the Application, Installation, and Maintenance of Solid State Control" and to NEMA ICS 7.1 (latest edition), "Safety Standards for Construction and Guide for Selection, Installation and Operation of Adjustable-Speed Drive Systems" or their equivalent governing your particular location.

WARNING

UNINTENDED EQUIPMENT OPERATION

  • Only use software approved by Schneider Electric for use with this equipment.

  • Update your application program every time you change the phys­ical hardware configuration.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Pay particular attention in conforming to any safety information, different electrical requirements, and normative standards that would apply to your adaptation.

WARNING

UNINTENDED EQUIPMENT OPERATION

Perform an in-depth risk analysis to determine the appropriate safety integrity level for your specific application, based on all the applicable standards.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Terminology Derived from Standards

The technical terms, terminology, symbols and the corresponding descriptions in this manual, or that appear in or on the products them­selves, are generally derived from the terms or definitions of interna­tional standards.

In the area of functional safety systems, drives and general automation, this may include, but is not limited to, terms such as safety, safety-related function, safe state, fault, fault reset, malfunction, failure, error, error message, dangerous, etc.

Among others, these standards include:

Standard

Description

IEC 61131-2:2007

Programmable controllers, part 2: Equipment requirements and tests.

ISO 13849-1:2015

Safety of machinery: Safety related parts of control systems.

General principles for design.

EN 61496-1:2013

Safety of machinery: Electro-sensitive protective equipment.

Part 1: General requirements and tests.

ISO 12100:2010

Safety of machinery - General principles for design - Risk assessment and risk reduction

EN 60204-1:2006

Safety of machinery - Electrical equipment of machines - Part 1: General requirements

ISO 14119:2013

Safety of machinery - Interlocking devices associated with guards - Principles for design and selection

ISO 13850:2015

Safety of machinery - Emergency stop - Principles for design

IEC 62061:2015

Safety of machinery - Functional safety of safety-related electrical, electronic, and electronic programmable control systems

IEC 61508-1:2010

Functional safety of electrical/electronic/programmable electronic safety-related systems: General requirements.

IEC 61508-2:2010

Functional safety of electrical/electronic/programmable electronic safety-related systems: Requirements for electrical/electronic/programmable electronic safety-related systems.

IEC 61508-3:2010

Functional safety of electrical/electronic/programmable electronic safety-related systems: Software requirements.

IEC 61784-3:2016

Industrial communication networks - Profiles - Part 3: Functional safety fieldbuses - General rules and profile definitions.

2006/42/EC

Machinery Directive

2014/30/EU

Electromagnetic Compatibility Directive

2014/35/EU

Low Voltage Directive

In addition, terms used in the present document may tangentially be used as they are derived from other standards such as:

Standard

Description

IEC 60034 series

Rotating electrical machines

IEC 61800 series

Adjustable speed electrical power drive systems

IEC 61158 series

Digital data communications for measurement and control – Fieldbus for use in industrial control systems

Finally, the term zone of operation may be used in conjunction with the description of specific hazards, and is defined as it is for a hazard zone or danger zone in the EC Machinery Directive (2006/42/EC) and ISO 12100:2010.

NOTE:

The aforementioned standards may or may not apply to the specific products cited in the present documentation. For more information concerning the individual standards applicable to the products described herein, see the char­acteristics tables for those product references.

If not otherwise stated, the respective terms are used in keeping with the IEC 61508 standard.