Filtering the Event Log

 

The 'Filter options' dialog appears after clicking the 'Filter' button in the event log dialogs. It is used to filter the present event log in order to show only a particular subset of entries.

NOTE:

The system event log can only be filtered for the 'User'.

Filter option

Meaning

Log Events

Only log-related events in the log are displayed (e.g., resets of the event log).

Project Events

Only project-related events in the log are displayed (e.g., insertion or deletion of libraries).

POU Events

Only POU-related events in the log are displayed (e.g., insertion or deletion of POUs).

Device parameterization Events

Only device parameterization-related events in the log are displayed (e.g., modifying the configuration of safety-related I/O devices).

SafePLC Events

Only error messages received from the Safety Logic Controller error stack are displayed.

Bus Navigator Events

Only Bus Navigator-related events are displayed (e.g., changing the Safety Logic Controller).

User

Only event log entries of this particular user are displayed.