Event and Error Log

 

While working with EcoStruxure Machine Expert - Safety, user actions are logged in event log files. Two different log types exist:

Every event log entry contains the following information:

Both the project event log and the system event log can be exported to a file (*.eve) which can be imported and opened later for inspection purposes. To clear the event logs, a reset function is available. After resetting an event log only one entry remains in the list logging the user who has performed the reset. Additionally, the event log lists can be filtered and sorted by different criterions.

NOTE:

Resetting the event log is only possible if you are logged-on at 'Development' level (see topic "Password  protection").

To open the event log, select 'File > Event Log...'. The event log dialog can either display project events or system events (switchable using the 'Project Events'/'System Events' button).

The following events are logged in the project event log/system event log and can be handled using the dialogs 'Project Event Log'/'System Event Log':

Logged event

Event group

Event log reset

Event log

New user project created

User project

CRC of user project modified (after compiling)

User project

User project downloaded to Safety Logic Controller

User project

Global variable declaration modified

User project

User project compiled

User project

Library included

User project

Library deleted

User project

Project certified

User project

Local variable declaration of a POU modified

POU

Code worksheet edited

POU

New POU inserted

POU

POU deleted

POU

POU renamed

POU

POU verification set/withdrawn

POU

Device parameter modified

Device parameterization

Device added

Device parameterization

Device removed

Device parameterization

Device type modified

Device parameterization

Error from the Safety Logic Controller error catalog

SafePLC