Inserting Comments - 'Comment' Dialog

 

Comments are descriptive texts for documentation purposes. You can insert comments at any position in FBD/LD code worksheets or assign them to an LD network. Comments may overlap other objects.

Comments are inserted/edited using the 'Comment' dialog.

Dialog element

Meaning

Comment

Comment text.

Font >>

Calls the 'Font selection' dialog where you can modify the font, font size, etc.

Add frame

The comment appears in the worksheet with a frame.

How to...

How to insert "free" comments

  1. Left-click at the desired worksheet position.

  2. Select 'Objects > Text (Comment)...' or click the 'Comment' icon on the toolbar.

  3. In the 'Comment' dialog, enter a comment and modify the font if desired.

    The general editing functions of the comment editor are described below.

How to insert network comments associated to an LD network

Network comments are automatically assigned to and displayed at the left power rail of an LD network.

  1. Double-click on the left power rail.

  2. In the 'Comment' dialog, enter a comment and modify the font if desired.

    The general editing functions of the comment editor are described below.

Functions of the comment editor

The 'Comment' dialog provides the basic editing functions of a standard text editor: