Opening a Project

 

The safety-related project relating to a Safety Logic Controller is auto­matically opened when starting EcoStruxure Machine Expert - Safety in the EcoStruxure Machine Expert 'Devices' tree for that particular Safety Logic Controller (context menu item 'EcoStruxure Machine Expert - Safety  > Start EcoStruxure Machine Expert - Safety'). There is no 'File open' menu item/toolbar icon available in EcoStruxure Machine Expert - Safety.

NOTE:

Message box 'Absolute project path is too long!'

The absolute path length to the directory containing the safety-related project is limited to a maximum of 255 characters. If a project is, for example, stored on a network drive in a deeply nested directory struc­ture, EcoStruxure Machine Expert - Safety may be unable to open the project. A message box informs you about the exceeded path length.

As the safety-related project is part of the standard project (contained in a subfolder), you have to save the EcoStruxure Machine Expert stan­dard project in another directory with a shorter absolute path.

When opening the safety-related project, the list of safety-related devices is synchronized between EcoStruxure Machine Expert and EcoStruxure Machine Expert - Safety. If any inconsistencies between the EcoStruxure Machine Expert 'Devices' tree and the EcoStruxure Machine Expert - Safety device tree are detected (because the bus configuration has been modified by deleting, adding or replacing safety-related devices in EcoStruxure Machine Expert), you have to (1) confirm each modification in a dialog referred to as 'Confirm changed SDIO Devices' and then (2) confirm the dialog with 'OK' as shown in the figure below.

Dlg_ChangedIO_Devices.gif

NOTE:

EcoStruxure Machine Expert - Safety project is part of EcoStruxure Machine Expert project:

After closing the safety-related project or exiting EcoStruxure Machine Expert - Safety, the safety-related project is automatically integrated into the EcoStruxure Machine Expert project. If you have edited an already existing safety-related project, the EcoStruxure Machine Expert project is updated accordingly by these modifications.