Monitoring/Evaluating Diagnostic Information of the Machine

 

The Safety Logic Controller as well as the safety-related I/O modules are able to determine and report their operational state. They can, for example, detect disturbances or irregular module behavior, such as short-circuits or EMC disturbance on their output channels.

Such module conditions may lead to a disabled functional machine component while non-affected components remain in an operational state. If, for example, an actuator cannot function as intended due to such a situation, hazards may result for persons and equipment and the machine must be set to the defined safe state. Refer to the hazard message below.

Affected modules indicate via the I/O channel LED indicator that an error has been detected by displaying a steady red indication, and by setting the related diagnostic process data item (e.g., SafeChannelOKxx) to SAFEFALSE. To detect such conditions and situations within your appli­cation, these process data items must be evaluated as shown in the application programming example below.

The process data items for diagnostic purposes provided by the safety-related I/O modules and the Safety Logic Controller help detect:

By evaluating these process data items provided by the Safety Logic Controller and the I/O modules involved in your safety-related applica­tion, i.e., by monitoring and processing the diagnostic controller/module information in the safety-related application, EcoStruxure Machine Expert - Safety allows you to:

WARNING

UNINTENDED EQUIPMENT OPERATION

  • Include in your risk analysis the impact of individual disabled func­tional machine components with regard to the safety of the entire machine.

  • Verify that the relevant diagnostic process data items provided by the Safety Logic Controller and the I/O modules involved in your safety-related application are monitored and evaluated so that your safety-related application can determine the state of the functional safety-related system.

  • Validate that the machine is set to the application-specific defined safe state (according to your risk analysis) depending on the safety-related diagnostic process data evaluation.

  • Use appropriate safety interlocks where personnel and/or equip­ment hazards exist.

  • Validate the overall safety-related function and thoroughly test the application.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Application example

A TM5SDI4DFS safety-related input module is used for evaluating an emergency stop button to control a mains contactor via the first channel of a TM5SDO4TFS safety-related output module.

For this example, the Devices tree in EcoStruxure Machine Expert looks as follows:

SE_DeviceMonitoringExample_DeviceTree.png

The two-channel emergency stop button is connected to the first two channels of the input module.

In EcoStruxure Machine Expert - Safety, the input channels are param­eterized for equivalence monitoring by using the process data item Safe­EquivalentInput0102 in the safety-related logic (insertion via drag & drop).

SE_DeviceMonitoringExample_Safegrid.png

The diagnostic process data items SafeChannelOKxx of both modules are used to detect irregular behavior of input/output channels. In addi­tion, the SafeModuleOk signals indicate the communication status of the modules.

Depending on the safety-related module type, different diagnostic process data items are available. In case of digital I/O modules, the SafeChannelOKxxxx signals are relevant.

In the safety-related code, these process data items are evaluated as follows:

SE_DeviceMonitoringExample_Code.png

The SafeModuleOK and SafeChannelOKxx process data items are logi­cally AND'd thus writing a resulting SafeHardware_OK variable. This variable is in turn logically AND'd with the enable signal coming from the safety-related SF_EmergencyStop function block which evaluates the emergency stop button.

The variable TM5DO4DFS_Out01 is the logical result of the AND instruction. It is assigned to the physical output address of channel 1 of the output module and controls the mains contactor.

If any of the diagnostic process data items is switched to SAFEFALSE due to an inoperable device or a detected error on an input/output channel, the global I/O variable TM5DO4DFS_Out01 becomes SAFE­FALSE and de-energizes the mains contactor.

Therefore, the running operation of the controlled machine depends on both the deactivated emergency control button and the correct operation of the modules involved.

Generating diagnostic messages in the non-safety-related applica­tion EcoStruxure Machine Expert

The diagnostic process data items of the safety-related modules are mirrored as diagnostic bits in the LMC non-safety-related controller. This way, they are also available in EcoStruxure Machine Expert. To display safety-related module states in the HMI, these diagnostic bits must be processed accordingly in the non-safety-related application in order to generate an HMI message.

SE_DeviceMonitoringExample_StandardAppl.png 

The user-defined safety-related variable SafeHardware_OK used in our example can also be mapped to the non-safety-related LMC controller application. For that purpose, use the I/O mapping functionality IO configuration > SLC2LMS_NumberOfxxx of the Safety Logic Controller to generate a diagnostic message for, e.g., the HMI or Message Logger.

Resetting diagnostic states

There are different possibilities to reset a detected channel-related diag­nostic state after eliminating its cause:

Observe the following when setting an output channel: