Software requirements
To run EcoStruxure Machine Expert - Safety, one of the following operating systems must be installed:
Microsoft Windows 10 (system locale English/USA or German/Germany) without beta releases of patches installed.
Microsoft Windows 8/8.1 (system locale English/USA or German/Germany) with latest SP installed.
Microsoft Windows 7 (system locale English/USA or German/Germany) with latest SP installed.
Hardware requirements
To run EcoStruxure Machine Expert - Safety, the following workstation requirements must be fulfilled:
Device |
Minimum |
Recommended |
IBM compatible PC with Pentium processor |
1 GHz x86 architecture |
2 GHz x86 architecture |
System RAM |
1 GB |
2 GB |
Hard disk |
500 MB free memory space |
1 GB free memory space |
Color settings |
True color |
|
LAN connection |
required |