Overview on EcoStruxure Machine Expert - Safety features

EcoStruxure Machine Expert - Safety is based on the IEC 61131-3 stan­dard and is designed to meet the safety requirements defined in the IEC 61508 standard.

EcoStruxure Machine Expert - Safety is an extended level tool according to the PLCopen Safety Specification.

EcoStruxure Machine Expert - Safety includes the required tools for the various development phases of a Safety Logic Controller application:

These tools and functions are: