ADD / ADD_S - Addition for ANY_NUM or ANY_SAFENUM
This arithmetic function realizes an addition of the operands connected to the input parameters. It is available as standard function ADD and safety-related function ADD_S.
NOTE:
An overflow (i.e., 16-bit-overflow) results in an error. As a result, the Safety Logic Controller enters the Stop state.
ADD
|
Parameter |
Data types |
Description |
|
IN1 |
ANY_NUM |
Summand |
|
IN2 |
ANY_NUM |
Summand |
|
OUT |
ANY_NUM |
Sum |
ADD_S
|
Parameter |
Data types |
Description |
|
IN1 |
ANY_SAFENUM |
Summand |
|
IN2 |
ANY_SAFENUM |
Summand |
|
OUT |
ANY_SAFENUM |
Sum |
NOTE:
All parameters must have the same data type.