This bitwise Boolean function realizes a logical AND integration of the operands connected to the input parameters. It is available as standard function AND and safety-related function AND_S.
AND
Parameter |
Data types |
Description |
IN1 |
ANY_BIT |
Input value |
IN2 |
ANY_BIT |
Input value |
OUT |
ANY_BIT |
Output value |
AND_S
Parameter |
Data types |
Description |
IN1 |
ANY_SAFEBIT |
Input value |
IN2 |
ANY_SAFEBIT |
Input value |
OUT |
ANY_SAFEBIT |
Output value |
NOTE:
Input parameters can be duplicated.
NOTE:
All parameters must have the same data type.