F_TRIG / F_TRIG_S - Falling edge detector
This edge detection function block detects a falling edge. If a falling edge is detected at the input CLK, the output Q changes from FALSE to TRUE. Q remains TRUE until the next call of the function block. If the function block is called for the first time, Q is FALSE until the first falling edge is detected.
The function block is available as standard function block F_TRIG and safety-related function block F_TRIG_S.
F_TRIG
|
Parameter |
Data types |
Description |
|
CLK |
BOOL |
Detects a falling edge |
|
Q |
BOOL |
If a falling edge is detected, Q changes from FALSE to TRUE |
F_TRIG_S
|
Parameter |
Data types |
Description |
|
CLK |
SAFEBOOL |
Detects a falling edge |
|
Q |
SAFEBOOL |
If a falling edge is detected, Q changes from FALSE to TRUE |
NOTE:
Function blocks have to be instantiated. Like variables, instances have to be declared before they can be inserted in a code body. Instances must be unique within the POU. In the following example, the instance name 'F_TRIG_S_1' is used for the F_TRIG_S FB.
Example for a safety-related function block declaration F_TRIG_S
Variables declarations in this example
NOTE:
If you want to use the standard function block F_TRIG in your code worksheet, you have to select the data type 'F_TRIG' for the function block instance in the local variables worksheet. Accordingly, the data type 'BOOL' must be used instead of 'SAFEBOOL'.