SEL / SEL_S - Selection of input
Depending on the value of the C (condition) input, this function selects one of its two inputs AT or AF and applies the related value to the SEL output.
If C = FALSE, the value at AF is applied at the SEL output. If C = TRUE, the value at AT is applied at the output OUT as shown in the following function table:
|
C input |
AT input |
AF input |
SEL/SEL_S output |
|
TRUE |
Value AT |
Value AF |
Value AT |
|
FALSE |
Value AT |
Value AF |
Value AF |
NOTE:
Although the SEL function supports all elementary data types that are available in the EcoStruxure Machine Expert - Safety, the inputs AT and AF as well as the SEL output must be connected to the same data type.
SEL
|
Parameter |
Data types |
Description |
|
C |
BOOL |
Condition which input is to be applied to the SEL output |
|
AT |
Value at the input is applied to the SEL output if C = TRUE |
|
|
AF |
Value at the input is applied to the SEL output if C = FALSE |
|
|
SEL |
Value at AT or AF, depending on C |
SEL_S
|
Parameter |
Data types |
Description |
|
C |
SAFEBOOL |
Condition which input is to be applied to the SEL output |
|
AT |
Value at the input is applied to the SEL output if C = TRUE |
|
|
AF |
Value at the input is applied to the SEL output if C = FALSE |
|
|
SEL |
Value at AT or AF, depending on C |