This standard bit manipulation function contained in the <BIT_UTIL> library writes the value applied at input LSB to the least significant Byte of the bit string applied at input DATA.
Parameter |
Data type |
Description |
LSB |
BYTE |
Value to be written to the LSB of DATA |
DATA |
WORD |
Input bit string to be modified |
OUT |
WORD |
Output bit string with modified written LSB |