FUNCTION CONCAT : STRING(255)
Concatenates two strings
CONCAT(STR1,STR2) means: Connect STR1 and STR2 to a single string STR1STR2.
(* Example declaration *)
VarSTRING1 : STRING ;
(* Example in ST , result is 'SUSIWILLI' *)
VarSTRING1 := CONCAT ('SUSI','WILLI');
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
CONCAT |
STRING(255) |
Concatenated string, max. 255 characters. If the result doesn't fit into these 255 bytes, it will be silently truncated. No error is produced. |
|
Input |
STR1 |
STRING(255) |
String 1 to be concatenated, max. 255 characters |
|
STR2 |
STRING(255) |
String 2 to be concatenated, max. 255 characters |