FUNCTION_BLOCK CTUD
Increments and decrements a given value
Note
Datatype WORD, which is used for PV in CODESYS, does not match the IEC standard, which for PV defines datatype INT.
(* Example declaration *)
CTUDInst : CUTD ;
(* Example in ST *)
CTUDInst(CU := VarBOOL1, CD:= VarBOOL2, RESET := VarBOOL3, LOAD:=VarBOOL4 , PV:= VarWORD1);
VarBOOL5 := CTUDInst.QU ;
VarBOOL6 := CTUDInst.QD ;
VarWORD2 := CTUDInst.CV ;
InOut:
|
Scope |
Name |
Type |
Comment |
|
Input |
CU |
BOOL |
Rising edge: Incrementing CV by one |
|
CD |
BOOL |
Rising edge: Decrementing CV by one |
|
|
RESET |
BOOL |
TRUE: Reset CV to 0 |
|
|
LOAD |
BOOL |
TRUE: Set CV to the start value PV |
|
|
PV |
WORD |
Start value for decrementing / upper limit for incrementing |
|
|
Output |
QU |
BOOL |
TRUE if CV >= PV |
|
QD |
BOOL |
TRUE if CV = 0 |
|
|
CV |
WORD |
Current counter value |