FUNCTION FIND : INT
Searches for the position of a partial string within a string.
FIND(STR1, STR2) means: Find the position of the first character where STR2 appears in STR1 for the first time. If STR2 is not found in STR1, then OUT:=0.
(* Example declaration *)
arINT1 : INT ;
(* Example in ST , result is '4' *)
arINT1 := FIND ('abcdef','de');
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
FIND |
INT |
Character position of the first occurance of STR2 in STR1. If no occurance is found, result is 0 |
|
Input |
STR1 |
STRING(255) |
String within which STR2 is searched |
|
STR2 |
STRING(255) |
String whose position is searched in STR1 |