PreventaSupport - Library Guide
This document describes the function blocks FB_PreventaDiag and FB_PreventaMain. FB_PreventaDiag can be used
to evaluate the diagnostic output of Preventa XPS safety modules, thus monitoring the
device functionality by translating the bit sequence into diagnostic code. FB_PreventaMain uses this diagnostic
code as input and executes calculations concerning maintenance tasks based on the code.
NOTE: This help is only available in English.