TYPE PROC_CMD :
This enumeration is used when working with asynchronous methods. The current state is issued with the data structure PROC_STATE
InOut:
|
Name |
Initial |
Comment |
|
0 |
Operation is not started and stays in IDLE mode. The operation is returned to its initial state. |
|
|
Operation is started upon a rising edge and executed as long as the input remains on EXECUTE. The operation is done as soon as the output is assigned the value PROC_STATE.DONE. |
||
|
Operation is aborted. The abort is done if the state is assigned the value PROC_STATE.ABORTED. |